|
Supported Operating System |
Supported Database Options |
|---|---|
|
Windows® Server® 2019 (version 1809 or later) (64-bit) Windows® Server® 2016 (version 1607 or later) (64-bit) |
SQL Server® 2019 with CU19 (64-bit) SQL Server® 2017 with CU31 (64-bit) SQL Server® 2016 with SP3 GDR (64-bit) |
Use the steps in the following table for upgrading the database component of the ADX on a split Metasys system.
|
Step |
Action |
Reference or Additional Steps |
|---|---|---|
|
1. |
Verify that the currently installed version of SQL Server software is supported for the new release of Metasys software. If necessary, apply the supported service pack or cumulative update. |
See Verifying your computer has a supported version of SQL Server software installed. |
|
2. |
Install the Metasys Database Manager to Release 12.0.50. Metasys Database Manager and the Metasys Server software must be at the same release. |
Refer to the Metasys Database Manager Installation Guide (LIT-12011553) . |
|
3. |
(Optional) If you need the server to be FIPS compliant, enable FIPS mode and install the Metasys FIPS component. |
|
|
4. |
Create a full disk image backup of the computer's hard drive to external media (optional but recommended). |
Refer to the documentation that came with your operating system backup software. |
|
5. |
Go to the next section to upgrade the web/application server of the split ADX. |
Go to Web/Application Server. |