Supported Operating System |
Supported Database Options |
---|---|
Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit). For all future Windows 10 updates after version 22H2, Johnson Controls will evaluate and certify that Metasys software can support the updates before we provide guidance on support. |
SQL Server® 2019 Express with CU19 (64-bit) SQL Server® 2017 Express with CU31 (64-bit) SQL Server® 2016 Express with SP3 GDR (64-bit) |
Use the steps in the following table for upgrading the Metasys Server software on a computer with a desktop operating system.
Step |
Action |
Reference or Additional Steps |
---|---|---|
1. |
Create a full disk image backup of the computer's hard drive to external media before upgrading any Metasys software (optional but recommended). |
Refer to the documentation that came with your operating system backup software. |
2. |
Check if the computer has a SHA256 self-signed certificate bound to Default Web Site in IIS. If the Metasys Server computer has a purchased certificate from a certificate authority (CA), determine if this is a SHA256 (Secure Hash Algorithm) certificate. If so, follow the steps on the right. If not, skip to the next step. Also, for more details, refer to the Network and IT Guidance Technical Bulletin (LIT-12011279) . |
|
3. |
Upload and back up all Metasys Server and network engine archive databases to the existing SCT. Make sure you select the Include Security option for the upload. |
Refer to Database Uploading, Downloading, and Synchronization of SCT: System Configuration Tool Help (LIT-12011964) or the SCT Technical Bulletin (LIT-1201534) for the release you have currently installed (not the new release). |
4. |
Determine if you need to record
existing user accounts and roles:
|
Log in to SCT and open the Security Administrator tool (Tools > Administrator). In Security Administrator, record all roles, local user accounts, and Active Directory user accounts that you want to recreate in the upgraded SCT. All customized roles and user accounts are lost when you uninstall SCT 5.2 (or earlier) and install a newer version of SCT. For easy recall later, you may find it helpful to use the computer's print screen function to capture the user access permissions and other information for each role. Refer to the Metasys Site Management Portal Help (LIT-1201793) for Release 5.2 or earlier. |
5. |
Forward all trend samples from each network engine to the Metasys Server Site Director by using the Route Samples command at each engine. This step ensures that the Site Director has all possible samples before you begin the upgrade. Wait a few minutes to ensure that all samples have been forwarded. |
Refer to Metasys Site Management Portal Help (LIT-1201793) for information about the Route Samples command. |
6. |
Stop the Metasys III Device Manager service on the Metasys Server computer. This action prevents the collection of any new audits, alarms, trends, and annotations while you perform the upgrade. If the customer can accept the loss of data samples during an upgrade, you can skip to the next step. |
Right-click the Windows taskbar and start Task Manager. Click the Services tab. Locate a service called Metasys III Device Manager. Select this service and right-click and select Stop Service. The Metasys III Device Manager service stops. |
7. |
Perform a complete backup of all historical data in the Metasys Server computer with the Metasys Database Manager. If the system to be upgraded is at Release 8.0 or 8.1, after the historical databases are backed up, use the SQL Server Management Studio to backup the SpacesAuthorization database. After the installation is complete, restore the SpacesAuthorization database. |
Refer to Backing Up a Database in Metasys Database Manager Help (LIT-12011202) . |
8. |
Make a copy of each historical database backup file and archive backup file and store them on removable media for example, a flash drive or DVD. |
Use Windows Explorer to prepare and archive the file copies. |
9. |
Uninstall the Ready Access Portal software if currently installed. |
Refer to the Uninstalling Ready Access Portal Software section in the Ready Access Portal Software Installation Instructions (LIT-12011523) . |
10. |
Uninstall the NxE Information and Configuration Tool (NCT) if present. |
In Control Panel, click Programs > Programs and Features. Select the program from the list and click Uninstall. |
11. |
Uninstall the Metasys Export Utility software if currently installed. |
In Control Panel, click Programs > Programs and Features. Select the program from the list and click Uninstall. |
12. |
Select the appropriate action:
|
In Control Panel, click Programs > Programs and Features. Select the program from the list and click Uninstall. |
13. |
Select the appropriate action:
|
In Control Panel, click Programs > Programs and Features. Select the program from the list and click Uninstall. |
14. |
Select the appropriate action:
|
In Control Panel, click Programs > Programs and Features. Select Johnson Controls - Launcher from the list of programs and click Uninstall. |
15. |
Select the appropriate
action:
|
|
16. |
Uninstall the Metasys Database Manager if currently installed. |
Refer to the Metasys Database Manager Installation Guide (LIT-12011553) . |
17. |
Verify that the currently installed version of SQL Server software is supported for the new release of Metasys software. If necessary, apply the supported service pack or cumulative update. |
See Verifying your computer has a supported version of SQL Server software installed. |
18. |
Install or Upgrade the Metasys Server Software. |
To install, see Metasys Server Software. To upgrade, see Upgrading Metasys Server. |
19. |
Start Metasys UI to verify proper operation. |
Refer to their respective installation documents. For MVE, see Installing MVE Software. |
20. |
(Optional) License SMP software. Note: An SMP license is not required if MVE is
installed and licensed.
|
Refer to Metasys Software Purchase Options Product Bulletin (LIT-12011703) |
21. |
Start Launcher on the computer and launch the Site Management Portal (SMP) for the upgraded Metasys Server. |
Refer to Launcher Tool Help (LIT-12011742) . |
22. |
To verify Metasys Server operation, log in to the Metasys Server using the MetasysSysAgent user and password. |
|
23. |
Log on to SCT 15.0, then use the Manage Archive wizard to upgrade the ADS/ADX device to Release 12.0. When asked to enter the Metasys Server user credentials, specify the MetasysSysAgent user and password. If during the upgrade process an Upgrade Warning dialog box appears regarding password resets, set a default password for the affected users, then contact the users of their new default password. Each affected user is prompted to change this default password when logging on to the Metasys Server 12.0.50 for the first time. |
Refer to SCT: System Configuration Tool Help (LIT-12011964) . |
24. |
If you upgraded the ADS/ADX device in your SCT archive from a Metasys
version prior to Release 12.0, to Release 12.0, confirm the following:
|
To check the configuration of the Third party BBMDs, see Checking third party BBMDs compatibility for ADS/ADX upgrades. To check the configuration of the Email DDA destinations, see Checking email DDA compatibility for ADS/ADX upgrades.
Note: The archive download to a Release 12.0 ADS/ADX fails if these
attributes have an incompatible configuration. For more information, see General Troubleshooting.
|
25. |
Download the Site Director
archive database from SCT 15.0 to the Metasys Server Site Director, making sure that you
click Include Security. When asked to enter the Metasys Server user
credentials, specify the MetasysSysAgent user and password. If the login for the Metasys
Server fails, click the Clear Security Database tab and click Set to be cleared. The device is upgraded, but the security database
is removed from the archive.
Note: A Server download logs off Metasys
UI and SMP users.
Note: Before you attempt a
download/upload to the server from SCT, wait for it to become operational. If you perform
a download/upload before then, the server does not operate correctly. To fix this, restart
the Metasys server host, wait for it to become operational, and try the process
again.
|
Refer to Database Uploading, Downloading, and Synchronization in SCT: System Configuration Tool Help (LIT-12011964) for information on downloading. |
26. |
(Optional) If you want to move the Metasys historical databases now, use SQL Management Studio to move the databases to the desired location. |
See Moving Metasys Historical Databases to a Custom Location. |
27. |
Install the Metasys Database Manager to Release 12.0.50. Metasys Database Manager and the Metasys Server software must be at the same release. |
Refer to the Metasys Database Manager Installation Guide (LIT-12011553) . |
28. |
Update the network engines that
you want to upgrade to Release 12.0.
Note: If you are upgrading from
Release 5.2 or later, you do not need to update all devices to the newer release (except
the Site Director). SCT 15.0 supports devices at multiple Metasys software releases,
beginning with Release 5.2.
|
Refer to NAE Update Tool Help (LIT-12011524) and SCT: System Configuration Tool Help (LIT-12011964) . |
29. |
If you updated network engines to Release 12.0, use SCT 15.0 to download the archive database of each network engine. The download also restores the Security database. After the download completes, issue the Reset Device command to each downloaded N40-class device (NxE35, NIE39, NxE45, NIE49, NxE25, or NIE29s) to ensure that the security database is archived to non-volatile memory. This step is new beginning at Release 8.0, but is not required for any other network engine (for example, NxE55s, NxE59s, SNEs, and SNCs). |
Refer to Database Uploading, Downloading, and Synchronization in SCT: System Configuration Tool Help (LIT-12011964) for information on downloading. |
30. |
If you need to bind a
purchased SHA256 certificate from a public certificate authority, follow the steps on the
right.
Note: The purchased
certificate must be SHA256 to work with Metasys UI.
|
|
31. |
(OPTIONAL) If you need the server to be FIPS compliant, enable FIPS mode and install the Metasys FIPS component. |
|
32. |
Create a full disk image backup of the computer's hard drive to external media (optional but recommended). |
Refer to the documentation that came with your operating system backup software. |