Metasys Server In-Place Upgrade - Metasys - LIT-12012162 - MS-ADS05U-0 MS-ADX10U-0 MS-ADX10SQL-0 MS-ADX25U-0 MS-ADX25SQL-0 MS-ADX50U-0 MS-ADX50SQL-0 MS-ADX50SQL2-0 MS-ADX100U-0 MS-ADX100SQL2-0 - Server - Metasys Server - 12.0.50

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document number
LIT-12012162
Version
12.0.50
Revision date
2023-10-12
Product status
Active

This section includes the steps for performing an in-place upgrade of the ADS or ADX software to Metasys Server 12.0.50 An in-place upgrade is for upgrading an existing Metasys system on the same computer using the same version or upgraded version of SQL Server software. (This upgrade selection also applies if you need to update SQL Server software to a newer service pack.) Before upgrading to Metasys Server 12.0.50 software, make sure you review Pre-Work checklist for new installations and upgrades and Table 1.

Which type of Metasys Server are you upgrading?
Unified ADS Select to upgrade a Metasys Server on a desktop operating system.
Unified ADS with SCT Select to upgrade a Metasys Server and SCT on a desktop operating system.
Unified ADX Select to upgrade a Metasys Server on a server-class operating system.
Unified ADX with SCT Select to upgrade a Metasys Server and SCT on a server-class operating system.
Split ADX with SCT Select to upgrade a Metasys Server and SCT on a split configuration. With a split ADX, the database component is installed on one server-class system, the web/application component is installed on another server-class operating system, and SCT is installed on either a server-class or desktop operating system.