About this task
Note:
If a previous release of MVE software is installed on your computer, you need to uninstall
both the MVE software and ADX software and then reinstall the ADX and the new MVE
software. Go to Uninstalling MVE Software.
- Go to Software Manager and check if the licenses activated on the ADX support MVE. If there are any unsupported licenses activated on the ADX, use Software Manager to deactivate them. For a list of supported and unsupported licenses, refer to the Licensing for MVE sites versus non-MVE sites in the Metasys UI Help (LIT-12011953).
- Obtain the MVE installation file.
- Using Windows Explorer, browse to the location of the MVE installation file.
- Right-click MetasysforValidatedEnvironments_12.0.50.exe and select Run as Administrator. Enter the Administrator's user credentials if prompted. The setup window appears.
- On the Setup window, click Install.
- Under the Database section, select from these options:
-
SQL Instance
: Click the down
arrow to select the server name of the SQL database engine installed on the computer.
For a unified ADX, you select (localhost) in most cases.
However, if multiple SQL Server instances are found on the local server, click the one
to use for Metasys software. For a split ADX, input the database server name in this
format:
<servername>
(default instance) or<servername>\<database instance>
(named instance).Note: If your installation of SQL Server uses the default instance name, specify only the server name, but do not include the default instance name. Otherwise, an error message appears and you cannot proceed with the installation. You only need to specify a database instance if you have a named instance. Also, if the server name you specify does not resolve, use the server's IP address. - Windows Authentication : Select if you want the installer to use the Windows OS credentials of the currently logged-in user to access the SQL Server software. The logged-in user must be a member of the system administrators (sysadmin) role in SQL Server. After installation, you can remove the SQL Server software system administrator rights from this user if so directed by IT personnel.
- Username and Password : Clear the Use Windows Authentication box to enter the SQL Server Administrator login and password credentials in these fields if you want the installer to use a SQL Server login with system administrator rights.
-
SQL Instance
: Click the down
arrow to select the server name of the SQL database engine installed on the computer.
For a unified ADX, you select (localhost) in most cases.
However, if multiple SQL Server instances are found on the local server, click the one
to use for Metasys software. For a split ADX, input the database server name in this
format:
- When all installation steps have finished, the Metasys Validation Environment Setup Complete box appears. Click Restart Now to restart your computer. After the restart, continue with the next step.
- License the MVE software with the Software Manager. For licensing instructions, refer to the Software Manager Help (LIT-12012389).