Launching the User Interfaces - Metasys - LIT-12012162 - MS-ADS05U-0 MS-ADX10U-0 MS-ADX10SQL-0 MS-ADX25U-0 MS-ADX25SQL-0 MS-ADX50U-0 MS-ADX50SQL-0 MS-ADX50SQL2-0 MS-ADX100U-0 MS-ADX100SQL2-0 - Server - Metasys Server - 12.0.50

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document type
Installation Guide
Document number
LIT-12012162
Version
12.0.50
Revision date
2023-10-12
Product status
Active

This section covers the launching of the user interfaces that are installed with the Metasys Server software.

If you want to secure the launching of the SMP UI with the Warning Banner option, refer to Metasys Site Management Portal Help (LIT-1201793) for details on how to enable the Warning Banner option.

Note: We strongly recommend that you do not browse to the SMP UI from a computer running a server-class OS. By default, Windows Internet Explorer Enhanced Security Configuration is enabled on server-class operating systems, and may block the Launcher download page from access to the SMP. Open the SMP UI from a computer that is not running a server-class OS.