Software Component |
Product |
Where to Obtain |
|
---|---|---|---|
Operating System (select one) 1 |
|||
|
Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit). For all future Windows 10 updates after version 22H2, Johnson Controls will evaluate and certify that Metasys software can support the updates before we provide guidance on support. 2 |
ADS /SCT |
Microsoft Corporation |
|
Windows® Server® 2019 (version 1809 or later) (64-bit) |
ADX /SCT |
|
|
Windows® Server® 2016 (version 1607 or later) (64-bit) |
||
Operating System (OS) Components (installed by Metasys Server) |
|||
|
Internet Information Services (IIS) (included with OS) |
ADS/ADX /SCT |
OS media |
|
Microsoft Message Queuing (MSMQ) |
||
Miscellaneous (select all) |
|||
|
Microsoft .NET Framework 3.5 SP1 or 3.5.1 |
ADS/ADX /SCT |
OS Media |
Microsoft .NET Framework 6.0.6 (installed by Metasys Server) |
|||
|
Microsoft Silverlight® 5.0 or higher 3 |
Microsoft Silverlight is no longer supported. You can view the Graphics+ graphics in the Metasys UI. | |
Database (select one) |
|||
|
SQL Server® 2019 Express with CU19 (64-bit) |
ADS /SCT |
|
|
SQL Server® 2017 Express with CU31 (64-bit) |
||
|
SQL Server® 2016 Express with SP3 GDR (64-bit) |
||
|
SQL Server® 2019 with CU19 (64-bit) 4 (Standard or Enterprise Edition) |
ADX /SCT |
Microsoft Corporation |
|
SQL Server® 2017 with CU31 (64-bit) 4 (Standard or Enterprise Edition) |
||
|
SQL Server® 2016 with SP3 GDR (64-bit) 4 (Standard or Enterprise Edition) |
||
Database Tools |
|||
|
SQL Installer Tool |
ADS /SCT |
|
|
Microsoft SQL Server Management Studio |
||
Reporting Services |
|||
|
Microsoft Report Viewer 2012 Redistributable Package 5 |
ADX |
Before you begin with the Metasys Server installation or upgrade, review Table 1 to verify
that you have the required software. The table also indicates where you can obtain each software
component.
Note: If you purchased Metasys
Server software that includes SQL Server software (for example, MS-ADX25SQL-0), the SQL Server
package is provided in a .zip file. Simply use a file extraction tool such as WinZip™ or 7-Zip
File Manager to extract the .zip file to the server's hard drive.
Note: Do not install Metasys on a
Domain Controller. A Domain Controller provides the Active Directory service to network users
and computers; stores directory data; and manages user and domain interactions including the
login process, authentication, and directory searches.
1 We highly recommend that the
computer you want to use for Metasys software had its operating system installed on a
cleanly formatted hard disk. If you use a computer that was upgraded from a previous
version of Windows, files and registry settings left behind after the upgrade may
adversely affect the installation of Metasys system software.
2 Metasys system
software does not support the touchscreen interface that is featured in the Windows 10
operating system.
3 Required for viewing
Graphics+ files on Site Management Portal software clients.
4 At
Release 12.0.50, Metasys Advanced Reporting
System is compatible with SQL Server 2017, and SQL Server 2016 software, but is not compatible with SQL Server 2019.
5 Required for reports generated by the
Metasys Advanced Reporting System. Use Report Viewer 2012 Redistribution Package for both
SQL Server 2017 and SQL Server 2016 software.