Licensing - Metasys - LIT-12012162 - MS-ADS05U-0 MS-ADX10U-0 MS-ADX10SQL-0 MS-ADX25U-0 MS-ADX25SQL-0 MS-ADX50U-0 MS-ADX50SQL-0 MS-ADX50SQL2-0 MS-ADX100U-0 MS-ADX100SQL2-0 - Server - Metasys Server - 12.0.50

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document number
LIT-12012162
Version
12.0.50
Revision date
2023-10-12
Product status
Active

The Metasys Server requires a software license for its base product. An application called Software Manager, installed with Metasys Server software, manages Metasys software licenses on a machine. We recommend that you license Metasys Server software immediately after installation. Also installed with the Metasys Server is the Monitoring and Commanding API, which is an optional feature that you need to purchase and license separately. Metasys UI, however, does not require a separate license. For information about activating licenses, refer to the Starting a license activation section in the Software Manager Help (LIT-12012389).

Note: SMP UI access on a Metasys Server at Release 12.0 and later requires an SMP license except for an ADX with MVE installed and licensed.