The Metasys Server setup is a comprehensive utility that installs the Metasys Server, third-party components required by the Metasys Server software, and many of the Microsoft® Windows® components required by the Metasys system. The following tables list the components installed by the Metasys Server installer, unless already present. For the software listed under the Components and products not installed column, use the respective installation programs to add those components and applications.
Windows® components installed |
Metasys products installed |
Components and products not installed |
---|---|---|
|
|
|
Refer to the respective installation or upgrade tables for the steps to manually install .NET Framework 3.5.
Third-party component | Brief description |
---|---|
Erlang OTP 23.2 (11.1.4) | A required component for RabbitMQ functionality. |
RabbitMQ Server 3.8.16 | RabbitMQ is a service bus used to send notification messages to other services and is used for inter-process communication (messages) on the server. |
IP Address and Domain Restrictions | IIS module that applies rate limiting to Metasys API calls. This module and settings do not apply to SMP or Metasys UI. |
GraphDB | GraphDB stores a portion of the Metasys site's configuration data to improve data querying. |