Installing Metasys server for a non-English locale - Metasys - LIT-12012162 - MS-ADS05U-0 MS-ADX10U-0 MS-ADX10SQL-0 MS-ADX25U-0 MS-ADX25SQL-0 MS-ADX50U-0 MS-ADX50SQL-0 MS-ADX50SQL2-0 MS-ADX100U-0 MS-ADX100SQL2-0 - Server - Metasys Server - 12.0.50

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document number
LIT-12012162
Version
12.0.50
Revision date
2023-10-12
Product status
Active
If you are installing Metasys server software on a computer that is running a non-English locale, follow the steps outlined here before you start the installation.
  1. In Control Panel, click Clock, Language, and Region.
  2. Click Region (or Region and Language). The Region and Language window appears.
  3. Click the Administrative tab.
  4. In the Language for non-Unicode programs section, click Change system locale. Click Yes if prompted for consent. The screen for selecting the system locale appears.
  5. Select the desired language from the drop-down list. Click OK, then restart the computer for the changes to take effect.
  6. Install a supported edition of SQL Server software. For details, refer to the SQL Server Software Installation and Upgrade Instructions (LIT-12012240).
  7. Set the default language of SQL Server to match the locale set on the operating system as follows: Open SQL Server Management Studio and right-click the server instance name in Object Explorer. Click Properties. The Properties window appears.
  8. Click Advanced and set the Default Language property to the language you need. For more details, click here to read a Microsoft article about local language versions of SQL Server.
  9. Click OK and exit SQL Server Management Studio.
  10. After you install the Metasys Server software, use the Language Installation Program (LIP) to set the language on Metasys software. Refer to the Language Installation Program Help (LIT-12011349).