See Table 1 for general troubleshooting information. If you are troubleshooting an ADX with Metasys Advanced Reporting System, see Metasys Advanced Reporting System Troubleshooting.
Problem |
Solution |
||
---|---|---|---|
You experience installation problems and would like to consult the error log. |
The error messages are located in the following folder: C:\Users\<username>\AppData\Local Metasys_Server_x.x_<date>.html, where x.x is replaced by the release version number. |
||
During installation, you see the following error message:
|
Before you restart the computer, use the Metasys Post Install (MPI) Database tool to complete necessary data type conversion work. Refer to the Database Tools Commissioning Guide (LIT-12012254). |
||
During ADS/ADX installation, a RabbitMQ command prompt window opens that contains the following error text:
|
The computer has two instances of the RabbitMQ database. To resolve, open a Command prompt as Administrator and run the Enable_RabbitMQ_Management.bat script that is located in the following location on the ADS/ADX server: C:\ProgramData\Johnson Controls\MetasysIII\Diagnostics\Utilities |
||
During an ADX upgrade, you see the following error:
|
The JCIHistorianDB upgrade script timed out during ADX installation. Ordinarily, this script completes within a few seconds, but it may take longer if the existing JCIHistorianDB is very large or the server is busy with other activities. If this timeout occurs during ADX installation, uninstall the ADX, restart, wait 5 to 10 minutes, and then reinstall ADX. |
||
After a successful ADS/X upgrade, you see the following content under the View Status option:
|
The device upgrade process lists the user names whose passwords were updated to the default password that you specified when you performed the upgrade. Each user enters this default password upon initial log in, then defines a new password when prompted. |
||
During an ADS/ADX installation or upgrade, you see the following error:
|
This problem can occur on an ADX if SQL Server is not present or it is not running. Confirm that SQL Server is present and running before installing or upgrading an ADX. If you use Metasys UI version 1.5.1 or earlier, uninstall Metasys UI and try the installation or upgrade again. | ||
After an ADS/ADX upgrade, you see one of the following errors:
|
This problem occurs when the frameworkproperties.properties file does not update correctly. This file contains network parameters for ADS/ADX or ADS-Lite communication. To solve this problem:
Note: Do not change any other parameters. Also, do
not change the parameters above to values other than those noted
in this solution.
|
||
After an upgrade, one or more of the following happens:
|
This problem occurs because upgrades overwrite the .config files for the Metasys system. To retain custom settings related to the serial printer DDA, Metasys Advanced Reporting System refresh rate, and other system behavior, you must restore these customizations after each upgrade. Refer to the ADS/ADX Commissioning Guide (LIT-1201645). |
||
After an ADS/ADX upgrade, you see one of the following errors:
|
The event buffer of the network engine is almost full and the ADS/ADX cannot clear out the events. This issue may occur after the ADS/ADX is upgraded to new release but the network engine remains at an older release. To resolve, manually delete all the events from the network engine. |
||
After an ADS/ADX upgrade, Spaces or the Network tree do not appear when you log on to the Metasys UI. |
Allow one to two hours per 500 engines for the Online Archive to gather and fill the attributes and other data displayed in the Building Network tree. We recommend not accessing the Building Network tree objects and viewing the object's Detail widget during the initial startup and sync. Furthermore, do not issue Bulk Commands through the Advanced Search feature in the Metasys UI during initial startup and sync. |
||
During an ADS/ADX install or upgrade, one of the following errors appears on the screen for the Reporting tab:
|
For the first error, the specified user credentials are incorrect or the syntax used to specify the server name in the Server Name field is incorrect. The correct syntax is: <servername> (default instance) or <servername>\<database instance> (named instance). Valid examples: localhost 10.10.9.50 10.10.9.50\MySQLInstance For the second error, the archive name specified in the SCT Archive field is incorrect. |
||
During an ADS/ADX upgrade, the following messages appear:
|
As the result of FIPS 140-2 compliance introduced at Metasys Release 11.0, existing user accounts are affected. Cancel the upgrade process. Then, for each affected user, set a new password and verify that the Never Expire property under Account Policy is not set. The FipsLockUsers.txt file lists the user accounts that you need to fix. Additionally, for all other Metasys users, set a new password for any user who has not changed their password in more than two years. Then, restart the upgrade process. |
||
During an ADS/ADX install or upgrade, the following message appears:
|
The version of SQL Server currently installed is not compatible with the ADS/ADX at Release 12.0.50. Exit the installer and see Prerequisite Software Checklist for Installation and Upgrade for a list of supported versions of SQL Server. |
||
During an ADS/ADX install or upgrade, the following message appears:
|
This message is simply a notification that the version of SQL Server software currently installed on the computer is at the minimum level required for that version. The message is not prompting you to upgrade the SQL Server software that is currently installed on the computer. Click OK to continue with the installation, or click Cancel if you want to stop and upgrade to a later, supported version of SQL Server. |
||
An update error occurs when you are trying to install the ADX software on a split ADX system. |
A change from Microsoft made the Allow Updates server configuration option obsolete, adversely affecting the installation of ADX software. You need to execute a SQL Server script on the database server computer for a split ADX installation to work. Follow these steps:
|
||
This error message appears while uninstalling prior releases of ADS/ADX software:
|
The ADS/ADX uninstallation program could not locate and drop user g3-user. This situation does not affect the uninstallation. You can ignore the message. The ADS/ADX uninstallation should complete normally. |
||
When you uninstall the ADX with Metasys Advanced Reporting, you receive the following error message:
|
When this error occurs, the uninstall program could not remove the MetasysReports folder. Click OK to continue. After uninstalling the ADX software, manually delete the following folder and all its contents: C:\inetpub\wwwroot\MetasysReports |
||
When you uninstall the ADS/ADX, you receive the following error message:
|
When this error occurs, the uninstall program could not remove the ADS/ADX software because the Metasys FIPS component must be uninstalled from the computer. Remove the FIPS License Update first, (Uninstalling and unlicensing FIPS component), then remove the ADS/ADX software. |
||
You cannot browse from a client computer into the SMP UI or SCT UI on the ADS, ADS-Lite, or ADX . |
The computer's firewall settings may be set incorrectly. See Configuring the Windows Defender firewall for steps on how to configure the firewall. |
||
During the installation of Windows operating system features, a Windows Features dialog box appears that reads:
Two choices are given:
|
Windows is trying unsuccessfully to access the Internet to retrieve .NET Framework 3.5 files or other necessary updates. Select either choice and refer to the Windows support website for further instructions. |
||
When you try to navigate to a website using a server-class operating system with the Enhanced Security Configuration enabled, the Internet Explorer web browser displays a message box saying the content is blocked. |
Add the site to your web browser as a trusted site or disable Enhanced Security. To disable Enhanced Security for the server operating system, follow these steps:
|
||
The Metasys III Device Manager and Metasys III Action Queue services stop every time the services are started. The ADS/ADX is not functional. The Site Management Portal generates this error message:
|
The Windows server computer The services may need to be explicitly allowed to run. Use the Security Configuration Wizard to identify the Metasys III Device Manager service and Metasys III Action Queue service as Windows services that are allowed to run. |
||
This error may appear when a user is denied access to the ADS/ADX computer over the network. To resolve this problem:
|
|||
Anti-spyware software is installed on the computer and is not configured to allow the Metasys III Device Manager Service or Metasys III Action Queue Service to run; or, the anti-spyware software is not allowing the hosts file to be updated. Refer to the Network and IT Guidance Technical Bulletin (LIT-12011279). |
|||
You have a general problem with the SQL Server Software installation or upgrade (including error messages or non-functional tools). |
To resolve this problem:
|
||
Because SQL Server software versions and configurations vary, your upgrade procedure may differ from what is documented in Johnson Controls literature. If your upgrade does not follow the steps published in our literature and you are unsure about which selections to make, go to http://technet.microsoft.com/en-us/default.aspx for information. Perform a search based on the version of SQL Server software you want to install; for example, SQL Server 2019 or Upgrading to SQL Server 2019. |
|||
While using the SQL Installer tool, you receive a user or error message during SQL Server software installation or upgrade. Possible messages include:
|
Consult the error log file. The error messages file is located in the following folder: C:\Program Files\Microsoft SQL Server\<number based on the SQL release>\Setup Bootstrap\Log\Summary.txt Correct the problem and try the SQL Server installation or upgrade again. |
||
While using the SQL Installer tool, you experience installation problems after you edit the text in the Command Line Options window of the SQL Installer. |
The text within the Command Line Options window contains errors. Correct the errors or restart the SQL Installer so that the Command Line Options window defaults to its original content. |
||
You are trying to upgrade a split ADX but do not know the SQL Server database instance name in use by the ADX. |
Log in to the database server of the split ADX. Start the Registry Editor (regedit). In the tree on the left, browse to HKEY_LOCAL_MACHINE\SOFTWARE\Johnson Controls\Metasys\ADS. The DBServer field displays the name of the SQL Server instance currently in use by the ADX. |
||
The ADS/ADX installation or upgrade fails and the following error message appears:
|
In the Control Panel, open the System Properties
window and verify that the Verify that the computer name meets
the following criteria:
If the computer name does not meet these criteria, change the computer name. Refer to the ADS/ADX Commissioning Guide (LIT-1201645). |
||
During installation of SQL Server Management Studio, you receive this error message:
|
You need to install Microsoft .NET Framework 3.5 before you install Microsoft SQL Server Management Studio software. Cancel the installation and install .NET Framework 3.5 first, then install SQL Server Management Studio software. |
||
During SNE or SNC commissioning, you find that you cannot change the JCI IP Address and Computer Name attributes at the same time. |
For SNE and SNC engines upgraded to Release 12.0, you cannot change the Computer Name and JCI IP Address at the same time. If you need to change both of these attributes, change one at a time. The engine resets after each operation. |
||
The ADS/ADX
software does not function correctly after you do one of the
following:
|
To correctly change your SQL Server software
outside the usual install or upgrade process, follow these
steps:
If you have already changed SQL Server software
without uninstalling the ADS/ADX
,
follow these steps:
|
||
After upgrading to a newer version of SQL Server, ADS/ADX no longer starts. |
To correctly change your SQL Server software
outside the usual install or upgrade process, follow these
steps:
If you have already changed SQL Server software
without uninstalling the ADS/ADX
, follow these steps:
|
||
If you back up a database using a newer version of SQL Server software, you cannot restore the database on a system using any older version of SQL Server software. |
After you convert databases created with an older version of SQL Server software to a newer version of SQL Server software, you cannot go back to the older format. Two different SQL Server software formats cannot coexist on the same computer. If you have some customers who use the older version of SQL software and some customers who use the newer version of SQL software, you must maintain the SQL software versions on separate computers. You can work around this issue by downloading from a system running a newer version of SQL Server software and then uploading the archive into a system running an older version of SQL Server software. |
||
During an installation or upgrade of SQL Server Express, you may see a reference to a file named sqlncli.msi or the following error message:
|
To resolve this error:
|
||
The ADS/ADX does not start. |
Follow these steps to verify the correct SQL
Server software protocols are enabled:
|
||
The following error appears when you try to log in to the ADS/ADX :
|
If this server is running at an MVE site, the Active Directory single sign-on (SSO) feature is not available for the ADX UI (per design).
Alternatively, t
he user account settings for the
Active Directory may be invalid. To work around this problem,
follow these steps:
|
||
The following error appears when you try to log in to the ADS/ADX :
|
Solution 1: The Internet Explorer web browser proxy setting is set to bypass the proxy server for local addresses. To resolve this problem, start the browser and select Connections tab, then LAN Settings. On the Local Area Network Settings window, select Automatically Detect Settings and select Use automatic configuration script. Type the address of the proxy server. Then, clear both check boxes under the Proxy server section. Relaunch the browser. . Click theSolution 2: The URL of the ADS/ADX you entered included a space. Remove the space and reload the page. Solution 3: The Launcher is configured to use a proxy server, even though the network does not require a proxy server. Open the Launcher and click the Network Settings button. On the Network Settings window, select Use browser settings. Solution 4: Microsoft SQL Server is not running. Start the SQL Server service with the SQL Server Configuration Manager. |
||
(cont.) |
Solution 5: SQL Server
is missing from the computer’s Path variable. To resolve this
problem, follow these steps:
Solution 6: The computer contains files from an earlier operating system or from an earlier version of Metasys software that is conflicting with the updated software. Verify that a folder with an older OS does not exist on the hard disk (for example, WINDOWS.OLD). Solution 7: The computer is using an older version of the Internet Explorer web browser. Upgrade the browser to version 11. |
||
A message box appears displaying the error
|
To avoid the Intranet Settings Turned Off dialog
box, open Windows Internet Explorer and click to clear the
Automatically detect intranet
network check box in . Select the following options:
|
||
The following error appears when you try to open ADS/ADX from the Launcher:
|
You are trying to use an older version of Launcher that is not compatible with this ADS/ADX release. Uninstall the old version of Launcher, then try again. Or to have the latest Launcher pushed to your computer directly from the ADS/ADX computer, open the browser and go to http://<server computer name or IP address>/launcher.msi. |
||
The following error appears when you try to log in to the ADS/ADX : Login failed: Device runtime status has not
been determined.
|
IIS applications are dependent on IIS logging. If you disable IIS logging then you will need to restart the server. |
||
After you upgrade the ADS or ADX device in an SCT archive to
Release 12.0 or later, the archive download fails. The status
details for the download failure from View Status in SCT’s ActionQ
lists messages similar to the following:
|
This issue is seen when the Third party BBMDs attribute (attribute ID 32591) of the site object (class ID 286) contains a value with an invalid/incompatible data type (status 33289). You may see this issue when upgrading an ADS or ADX from a release earlier than Release 12.0, to Release 12.0 or later. To correct this issue, follow the steps listed in Checking third party BBMDs compatibility for ADS/ADX upgrades and then retry the archive download. |
||
After upgrading the ADS or ADX device in an SCT archive to Release 12.0 or later, the archive download fails. The status details for the download failure (from View Status in SCT’s ActionQ) lists messages similar to the following:
and
|
This issue is seen when the Email DDA attribute (attribute ID 32568) of the ADS/ADX object (class ID 425) contains an illegal or incompatible character (status 272). You may see this issue when you upgrade an ADS or ADX from a release earlier than Release 12.0, to Release 12.0 or later. To correct this issue, follow the steps listed in Checking email DDA compatibility for ADS/ADX upgrades and then retry the archive download. |