Changing Advanced Security Enabled to False in SMP - Metasys - LIT-12012162 - MS-ADS05U-0 MS-ADX10U-0 MS-ADX10SQL-0 MS-ADX25U-0 MS-ADX25SQL-0 MS-ADX50U-0 MS-ADX50SQL-0 MS-ADX50SQL2-0 MS-ADX100U-0 MS-ADX100SQL2-0 - Server - Metasys Server - 12.0.50

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document type
Installation Guide
Document number
LIT-12012162
Version
12.0.50
Revision date
2023-10-12
Product status
Active

About this task

To change the Advanced Security Enabled attribute to False with the SMP UI, follow these steps:

Procedure

  1. Log on to the Site Management Portal of the Site Director.
  2. Open the Site View for the Site Director.
  3. With Advanced selected, click Edit.
  4. Locate the Advanced Security Enabled attribute under the Operational Data section.
  5. Click the down arrow and select False.
    Figure 1. Changing the Advanced Security Enabled attribute
  6. Click Save. The server and engines across the entire site no longer use advanced security.
  7. As an option, use SCT to upload the Site Director so that this change is reflected in the database archive.
    Note: If some time later you change the Advanced Security Enabled attribute from False to True, a user message appears to indicate that all network engines prior to Release 10.0 are disconnected from the site because they can no longer communicate with the Site Director using advanced security. Do not set Advanced Security Enabled to True until all network engines are upgraded to Release 10.0 or later