Changing Advanced Security Enabled to False in Metasys UI - Metasys - LIT-12012162 - MS-ADS05U-0 MS-ADX10U-0 MS-ADX10SQL-0 MS-ADX25U-0 MS-ADX25SQL-0 MS-ADX50U-0 MS-ADX50SQL-0 MS-ADX50SQL2-0 MS-ADX100U-0 MS-ADX100SQL2-0 - Server - Metasys Server - 12.0.50

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document number
LIT-12012162
Version
12.0.50
Revision date
2023-10-12
Product status
Active

About this task

To change the Advanced Security Enabled attribute to False with the Metasys UI, follow these steps:

Procedure

  1. Log on to the Metasys UI of the Site Director.
  2. Navigate to the site object and display its Detail widget.
  3. Select the Site View tab.
  4. Locate the Advanced Security Enabled attribute under the Operational Data section.
  5. Click the attribute's linked value to open its edit field and then select False.
  6. Click the Save icon.