Welcome - Metasys - LIT-12012162 - MS-ADX10U-0 - MS-ADX50SQL-0 - MS-ADX10SQL-0 - MS-ADX50SQL2-0 - MS-ADX100SQL2-0 - MS-ADX100U-0 - MS-ADX25U-0 - MS-ADX50U-0 - MS-ADS05U-0 - MS-ADX25SQL-0 - Server - Metasys Server - 11.0

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document number
LIT-12012162
Version
11.0
Revision date
2021-07-02
Product status
Active

Welcome to the Metasys Server Installation and Upgrade Instructions. The document guides you through the steps you need to follow to install or upgrade the Metasys Server software. In this document, the Metasys Server is also referred to as the Application and Data Server (ADS) or the Extended Application and Data Server (ADX).