Licensing the Metasys Server Software - Metasys - LIT-12012162 - MS-ADX10U-0 - MS-ADX50SQL-0 - MS-ADX10SQL-0 - MS-ADX50SQL2-0 - MS-ADX100SQL2-0 - MS-ADX100U-0 - MS-ADX25U-0 - MS-ADX50U-0 - MS-ADS05U-0 - MS-ADX25SQL-0 - Server - Metasys Server - 11.0

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document number
LIT-12012162
Version
11.0
Revision date
2021-07-02
Product status
Active

The Metasys Server installation process also installs the Software Manager that you use to license the server and other Metasys applications. For information and instructions on how to properly license the Metasys ADS or Metasys ADX software, refer to the Software Manager Help (LIT-12012389)

After you license the Metasys ADS or Metasys ADX software, determine the next step as follows:

  • If the customer requires a FIPS compliant system, you must enable FIPS and install FIPS after you license the Metasys Server. Go to Enabling and installing FIPS component.
  • If operators at this facility use Graphics+ files, install Microsoft Silverlight 5, a software plug-in that is required to view graphics created with the Graphic Generation Tool. Go to Installing Microsoft Silverlight 5.
  • If this facility requires Metasys for Validated Environments software, go to Installing MVE Software.
  • If operators at this facility do not use Graphics+ files, the next step is to verify ADS/ADX installation. Go to Launching the User Interfaces.