Refer to the SCT Installation and Upgrade Instructions (LIT-12012067) for more information on supported platforms and for installing SCT.
Use the steps in the following table for upgrading SCT on a split Metasys system.
Step |
Action |
Reference or Additional Steps |
---|---|---|
1. |
Upload and back up all ADS/ADX and network engine archive databases to the existing SCT. Make sure you select the Include Security option for the upload. |
Refer to Database Uploading, Downloading, and Synchronization of Metasys SCT Help (LIT-12011964) or the SCT Technical Bulletin (LIT-1201534) for the release you have currently installed (not the new release). |
2. |
Forward all trend samples from each network engine to the ADS/ADX Site Director by using the Route Samples command at each engine. This step ensures that the Site Director has all possible samples before you begin the upgrade. Wait a few minutes to ensure that all samples have been forwarded. |
Refer to Metasys Site Management Portal Help (LIT-1201793) for information about the Route Samples command. |
3. |
Stop the Metasys III Device Manager service on the ADS/ADX computer. This action prevents the collection of any new audits, alarms, trends, and annotations while you perform the upgrade. If the customer can accept the loss of data samples during an upgrade, you can skip to the next step. |
Right-click the Windows taskbar and start Task Manager. Click the Services tab. Locate a service called Metasys III Device Manager. Select this service and right-click and select Stop Service. The Metasys III Device Manager service stops. |
4. |
Create a full disk image backup of the computer's hard drive to external media before upgrading any Metasys software (optional but recommended). |
Refer to the documentation that came with your operating system backup software. |
5. |
Uninstall the current version of Metasys Launcher from the SCT computer and all clients that log in to the ADS/ADX . |
In Control Panel, click Programs > Programs and Features. Select Johnson Controls - Launcher from the list of programs and click Uninstall. |
6. |
Select the appropriate action:
|
In Control Panel, click Programs > Programs and Features. Select the program from the list and click Uninstall. |
7. |
Select the appropriate action:
|
|
8. |
Select the appropriate
action:
|
|
9. |
Select the appropriate
action:
|
|
10. |
Start SCT from the Launcher or the Metasys SCT shortcut. Log in with the MetasysSysAgent user and password. The login process could take a little longer than usual. |
Refer to Launcher Tool Help (LIT-12011742) . |
11. |
Select the appropriate action:
|
Refer to the Security Administrator System Technical Bulletin (LIT-1201528) . |
12. |
Create a full disk image backup of the computer's hard drive to external media (optional but recommended). |
Refer to the documentation that came with your operating system backup software. |
13. |
Go to the next section to upgrade the database server of the split ADX. |
Go to Database Server. |