This section includes the steps for performing an out-of-place upgrade of the ADS or ADX software to Metasys Server Pre-Work checklist for new installations and upgrades and Out-of-Place Upgrade Considerations.
. An out-of-place upgrade applies in either of these two scenarios: (1) you need to reformat the computer that is currently running the Metasys system to a new, supported Windows operating system before performing the upgrade or (2) you need to move the current Metasys system to a different computer or virtual machine during the upgrade. Before upgrading to Metasys Server software, make sure you reviewWhich type of Metasys Server are you upgrading? | |
---|---|
Unified ADS | Select to upgrade a Metasys Server on a desktop operating system. |
Unified ADS with SCT | Select to upgrade a Metasys Server and SCT on a desktop operating system. |
Unified ADX | Select to upgrade a Metasys Server on a server-class operating system. |
Unified ADX with SCT | Select to upgrade a Metasys Server and SCT on a server-class operating system. |
Split ADX with SCT | Select to upgrade a Metasys Server and SCT on a split configuration. With a split ADX, the database component is installed on one server-class system, the web/application component is installed on another server-class operating system, and SCT is installed on either a server-class or desktop operating system. |