Metasys Server Installation - Metasys - LIT-12012162 - MS-ADX10U-0 - MS-ADX50SQL-0 - MS-ADX10SQL-0 - MS-ADX50SQL2-0 - MS-ADX100SQL2-0 - MS-ADX100U-0 - MS-ADX25U-0 - MS-ADX50U-0 - MS-ADS05U-0 - MS-ADX25SQL-0 - Server - Metasys Server - 11.0

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document type
Installation Guide
Document number
LIT-12012162
Version
11.0
Revision date
2021-07-02
Product status
Active

This section includes the steps for installing Metasys Server software. Before you begin the installation process, make sure you review Pre-Work checklist for new installations and upgrades.

If you instead need to upgrade existing Metasys Server software, see Metasys Server In-Place Upgrade or Metasys Server Out-of-Place Upgrade.

Which type of Metasys Server are you installing?
Unified ADS Select to install the Metasys Server on a desktop operating system.
Unified ADS with SCT Select to install the Metasys Server and SCT on a desktop operating system.
Unified ADX Select to install the Metasys Server on a server-class operating system.
Unified ADX with SCT Select to install the Metasys Server and SCT on a server-class operating system.
Split ADX with SCT Select to install a split Metasys Server where database component is installed on one server-class system, the web/application component is installed on another server-class operating system, and SCT is installed on a desktop or server-class operating system.