Refer to the SCT Installation and Upgrade Instructions (LIT-12012067) for more information on supported platforms and for installing SCT.
Use the steps in the following table for upgrading SCT on a split Metasys system.
Step |
Action |
Reference or Additional Steps |
---|---|---|
1. |
Upload and back up all ADS/ADX and network engine archive databases to the existing SCT. Make sure you select the Include Security option for the upload. |
Refer to Database Uploading, Downloading, and Synchronization of Metasys SCT Help (LIT-12011964) or the SCT Technical Bulletin (LIT-1201534) for the release you have currently installed (not the new release). |
2. |
Determine if you need to record
existing user accounts and roles:
|
Log in to SCT and open the Security Administrator tool (Tools > Administrator). In Security Administrator, record all roles, local user accounts, and Active Directory user accounts that you want to recreate in the upgraded SCT. All customized roles and user accounts are lost when you uninstall SCT 5.2 (or earlier) and install a newer version of SCT. For easy recall later, you may find it helpful to use the computer's print screen function to capture the user access permissions and other information for each role. Refer to the Metasys Site Management Portal Help (LIT-1201793) for Release 5.2 or earlier. |
3. |
Forward all trend samples from each network engine to the ADS/ADX Site Director by using the Route Samples command at each engine. This step ensures that the Site Director has all possible samples before you begin the upgrade. Wait a few minutes to ensure that all samples have been forwarded. |
Refer to Metasys Site Management Portal Help (LIT-1201793) for information about the Route Samples command. |
4. |
Stop the Metasys III Device Manager service on the ADS/ADX computer. This action prevents the collection of any new audits, alarms, trends, and annotations while you perform the upgrade. If the customer can accept the loss of data samples during an upgrade, you can skip to the next step. |
Right-click the Windows taskbar and start Task Manager. Click the Services tab. Locate a service called Metasys III Device Manager. Select this service and right-click and select Stop Service. The Metasys III Device Manager service stops. |
5. |
Perform a complete backup of all historical data in the ADS/ADX computer with the Metasys Database Manager. If the system to be upgraded is at Release 8.0 or 8.1, after the historical databases are backed up, use the SQL Server Management Studio to backup the SpacesAuthorization database. |
Refer to Backing Up a Database in Metasys Database Manager Help (LIT-12011202) . |
6. |
Make a copy of each historical database backup file and archive backup file and store them on removable media (for example, a flash drive or DVD). |
Use Windows Explorer to prepare and archive the file copies. |
7. |
Create a full disk image backup of the computer's hard drive to external media before upgrading any Metasys software (optional but recommended). |
Refer to the documentation that came with your operating system backup software. |
8. |
Select the appropriate action:
|
In Control Panel, click Programs > Programs and Features. Select the program from the list and click Uninstall. |
9. |
Uninstall the NxE Information and Configuration Tool (NCT) if present. |
In Control Panel, click Programs > Programs and Features. Select the program from the list and click Uninstall. |
10. |
Select the appropriate action:
|
|
11. |
Uninstall the current version of Metasys Launcher from the SCT computer and remove from all clients that log in to the ADS/ADX . |
In Control Panel, click Programs > Programs and Features. Select Johnson Controls - Launcher from the list of programs and click Uninstall. |
12. |
Select the appropriate
action:
|
|
13. |
Select the appropriate
action:
|
|
14. |
Start SCT from the Launcher or the Metasys SCT shortcut. Log in with the MetasysSysAgent user and password. The login process could take a little longer than usual. |
Refer to Launcher Tool Help (LIT-12011742) . |
15. |
As part of the in-place upgrade, open the archive database with SCT by clicking Item > Open Archive. See the information on the right. |
Select the
appropriate action:
|
16. |
Select the appropriate action:
|
Refer to the Security Administrator System Technical Bulletin (LIT-1201528) . |
17. |
Create a full disk image backup of the computer's hard drive to external media (optional but recommended). |
Refer to the documentation that came with your operating system backup software. |
18. |
Go to the next section to upgrade the database server of the split ADX. |
Go to Database Server. |