Launching the Metasys UI - Metasys - LIT-12012162 - MS-ADS05U-0 - MS-ADX100SQL2-0 - MS-ADX100U-0 - MS-ADX10SQL-0 - MS-ADX10U-0 - MS-ADX25SQL-0 - MS-ADX25U-0 - MS-ADX50SQL-0 - MS-ADX50SQL2-0 - MS-ADX50U-0 - Server - Metasys Server - 11.0

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document type
Installation Guide
Document number
LIT-12012162
Version
11.0
Revision date
2021-07-02
Product status
Active

To access the Metasys UI remotely from any client device, ensure that you have access to the Metasys Site Director (Internet, intranet, or Virtual Private Network (VPN) access) and browse to https://[SERVERNAME]/UI, where [SERVERNAME] is replaced with the hostname or IP address of your Metasys Site Director.

When you browse to the Metasys UI, your web browser displays a security certificate warning. The browser displays this warning if your Metasys UI site does not have a trusted security certificate.

If you see this warning, you can browse to the Metasys UI site by doing the following:
  • For Google Chrome, (1) tap or click Advanced; (2) Tap or click Proceed to [IP Address], where [SERVERNAME or IP Address] is the server name or IP address of the Site Director.
  • For Windows Internet Explorer, click Continue to this website (not recommended).
  • For Microsoft Edge, click Continue to this website (not recommended).
  • For Apple Safari, tap or click Continue in the Cannot Verify Sever Identity window.

The Metasys UI login screen appears. Enter your Metasys SMP login credentials.