Launching the Metasys Advanced Reporting System UI - Metasys - LIT-12012162 - MS-ADX10U-0 - MS-ADX50SQL-0 - MS-ADX10SQL-0 - MS-ADX50SQL2-0 - MS-ADX100SQL2-0 - MS-ADX100U-0 - MS-ADX25U-0 - MS-ADX50U-0 - MS-ADS05U-0 - MS-ADX25SQL-0 - Server - Metasys Server - 11.0

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document type
Installation Guide
Document number
LIT-12012162
Version
11.0
Revision date
2021-07-02
Product status
Active

You must log in to the ADX SMP UI and accept the license agreement before you access the Metasys Advanced Reporting System UI. This applies only to the first time you log in to the reporting system after an install or upgrade. See Launching the User Interfaces.

To launch the Metasys Advanced Reporting System UI, do one of the following:

  • In the SMP UI, select Tools > Advanced Reporting.

  • In Internet Explorer 11 or Microsoft Edge, browse to https://<hostname>/MetasysReports, where <hostname> is the computer name of the target ADX.

    Notes:
    • In Internet Explorer 11, select the Use Microsoft compatibility lists option, under Tools > Compatibility View Settings, to ensure that websites appear and function correctly.

    • Metasys Advanced Reporting System and Energy Essentials support Internet Explorer 11 on all computer platforms except on Windows 10. On Windows 10 computers, both Internet Explorer 11 and Microsoft® Edge® are supported.
  • Add the web address of the Metasys Advanced Reporting System to the Launcher, and use the Launcher to start the Metasys Advanced Reporting System UI.