To launch the ADS/ADX SMP UI, do one of the following:
-
On the ADS/ADX computer, from the Windows Start icon, go to Johnson Controls > Launcher. Follow the steps in Launcher Tool Help (LIT-12011742) to add a profile for the ADS/ADX under the SMP tab.
-
On the ADS/ADX computer, double-click the Metasys ADS or Metasys ADX icon on the desktop. Add a profile for ADS/ADX under the SMP tab by configuring the network credentials of the ADS/ADX computer. For details, refer to Launcher Tool Help (LIT-12011742) .
-
On another computer on the same network as the ADS/ADX computer, browse to https://<hostname>/metasys/, where <hostname> is the computer name of the target ADS/ADX.Note: If the message Missing Resource File appears when you try to open the ADS/ADX, prompt the server to push its version of the Launcher by browsing to https://<hostname>/launcher.msi.
Using the Launcher, configure the network credentials of the ADS/ADX computer to add its profile to the Launcher. For details, refer to the Launcher Tool Help (LIT-12011742) .
After you add the ADS/ADX, select it from the profile list under the SMP tab and click Launch. The SMP UI login screen appears. Log in with the MetasysSysAgent user name and default password. (For the default password, contact your local Johnson Controls representative.) You are forced to change the password to a valid, complex password the first time you log in to the ADS/ADX. Follow the password rules that appear in the Change Password dialog. For more information on passwords, refer to the Security Administrator System Technical Bulletin (LIT-1201528) .
For information on configuring and using ADS/ADX, refer to the ADS/ADX Commissioning Guide (LIT-1201645) and Metasys Site Management Portal Help (LIT-1201793) .