Configuring Virtual Machine for Metasys Server - Metasys - LIT-12012162 - MS-ADX10U-0 - MS-ADX50SQL-0 - MS-ADX10SQL-0 - MS-ADX50SQL2-0 - MS-ADX100SQL2-0 - MS-ADX100U-0 - MS-ADX25U-0 - MS-ADX50U-0 - MS-ADS05U-0 - MS-ADX25SQL-0 - Server - Metasys Server - 11.0

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document type
Installation Guide
Document number
LIT-12012162
Version
11.0
Revision date
2021-07-02
Product status
Active

If you are installing the Metasys Server software on a virtual machine (VM), verify the following before you start to install Metasys:

  • Ensure that the virtual machine is running in static memory mode, not dynamic. Otherwise, operational issues with SQL Server may occur.
  • If you are upgrading from a hardware server to a VM, configure the Metasys Server VM with the same amount of memory as the hardware server, or with at least 8 GB of memory.
  • Verify that the Process compatibility option under Virtual Machine Settings > Processor > Compatibility in Microsoft Hyper-V is not selected (Figure 1). For some Intel CPUs, this box is selected by default.
Figure 1. Processor compatibility setting on Metasys Server