Verifying the server certificate chain - Metasys - LIT-12012162 - MS-ADX10U-0 - MS-ADX50SQL-0 - MS-ADX10SQL-0 - MS-ADX50SQL2-0 - MS-ADX100SQL2-0 - MS-ADX100U-0 - MS-ADX25U-0 - MS-ADX50U-0 - MS-ADS05U-0 - MS-ADX25SQL-0 - Server - Metasys Server - 11.0

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document number
LIT-12012162
Version
11.0
Revision date
2021-07-02
Product status
Active

About this task

To verify a certificate chain for a Metasys server or SCT computer:

Procedure

  1. In Control Panel, select System and Security > Administrative Tools and double-click Internet Information Services (IIS) Manager. The IIS main screen appears.
  2. Highlight the name of the web server.
  3. Under the IIS section in the middle pane, double-click Server Certificates. The Server Certificates panel appears.
  4. On the Actions pane, click View. The Certificate screen appears.
  5. Click the Certification Path tab. The certificate chain appears.
  6. Click OK to close the certificate view.