Status Indicators - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

Status indicators show the status of items in the system on the user interface. For example, these status indicators appear in the navigation tree, in a column on Summary views, and in a column on the Global Search Viewer’s Search Results table. Also, a connection status indicator appears on the SCT login screen and Main screen to denote the current security level of the certificate. If you place the cursor over the icon, a tooltip appears to further describe the certificate. The following table shows examples of the status indicators and the mode in which they may appear.

Note: In Simulation mode, status indicators only appear in the Summary views in the display frame. The indicators do not appear in the navigation tree in this mode.
Table 1. Status Indicators

Indicator

Indicator Description

Status

Mode

Green Arrow

Item has been edited since it was last loaded to the Engine.

Offline

Blue Triangle

Local Site Director: Device is the Local Site Director.

Online

Offline

Green Shield with Check Mark

Communication between the client computer and the SCT computer is encrypted and trusted.

Online

Offline

Orange Shield with Exclamation Point

Communication between the client computer and the SCT computer is encrypted, but not trusted.

Online

Offline

Red Shield with X Symbol

Security level between the client computer and the SCT computer cannot be verified because the certificate has expired, is not valid, or is not present. However, if the client computer is using Launcher 1.6 and the SCT computer is at Release 11.1, communication is still encrypted.

Online

Offline