The screen contains four frames and provides a consistent look and feel in every mode (online, or offline). Your access to certain features depends on the mode in which you are operating and your assigned access type and privileges.
|
Number |
Name |
Description |
|---|---|---|
|
1 |
Menu |
Displays the menu bar and the first three characters of the logged-in user name. Active Directory service user names display as the fully qualified user name (for example, user@engineering.jci.com). Logging Out or exit from the system using buttons in the menu frame. |
|
2 |
Display |
Presents data or information in the user-selected Panel Layout. See the Display Frame Layout section for more information on the Display Frame. |
|
3 |
Navigation |
Displays navigation trees that organize items in the system. The All Items tree generates automatically when you configure the system database. You can create one or several user navigation trees (also referred to as user views) for defining your own navigation concept. For more information on the navigation tree, see the Navigation Tree section. |
|
4 |
Status |
Displays information about current user actions and the current time/time zone of the server that you are logged into (supervisory device or Site Director). |