Pop-up Menus - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Pop-up menus provide an efficient way to quickly access important item information. Pop-up menus are also referred to as right-click menus. To access pop-up menus, right-click an item in the Navigation Tree. Content of the menu depends on the type of selected item and your level of authorization. For example, point object pop-up menus usually show the options View, Command, Modify, and Show Extensions. For Engines, pop-up menus usually show View, Event Viewer, Audit Viewer, Command, Modify, Show Extensions, Alarm Report, Offline Report, Disabled Report, Operator Override Report, Supervisory Override Report, Trouble Report, Out of Service Report, and Remove from Site.