SCT in a Metasys Network - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Figure 1 shows SCT as part of an overall Metasys network. The SCT is installed on, and can be accessed by, a computer on the building network.

Figure 1. SCT as Part of a Metasys Network