Summary of Changes - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The following information is new or revised for SCT Release 13.2:

  • Added information in the Site Attributes, Download, and Upgrade/Migrate sections to state that if you have not manually set the Advanced Security Enabled attribute for a site to False, the previous default value of False changes to True after you upgrade to Metasys Release 10.1.
  • Added information about the SNE and SNC network engines. These network engines are new at Metasys Release 10.1.
  • Added information about the Background File Transfer feature, which you can use with Release 10.1 network engines.
  • Application and Data Server (ADS), Extended Application and Data Server (ADX), and Open Data Server (ODS) object attributes are now described in a single table. The table also lists the attributes of the Open Application Server (OAS) object, which is new at Metasys Release 10.1.
  • Added two new objects supported by the ODS at Release 10.1: Channel Object and Lighting Output Object.
  • Updated information regarding summary definitions and other content that you previously accessed through the Branch Purchase Package (BPP) and installation media. You now access this content through the License Portal.
  • Restructured troubleshooting section and added procedures.
  • Added product warranty and patent information at the end of the document.