Logic Tab - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2
Metasys SCT: System Configuration Tool Help
Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
The Logic tab appears on Program (Control System) objects, which are used for the LCT feature.