MS/TP Hardware Tab - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

Attributes associated with the hardware source for object data are shown under the Hardware tab of the display panel. Attributes marked with the letter C are configurable and attributes marked with the letter W are writeable.

Table 1. MS/TP Hardware Tab

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Baud Rate Selection

C,W

0

Uses MSTPDL Baud Rate

See the attribute description.

  • Auto: Uses baud rate of running network. This value is the recommended setting for everything on the FC bus except the bus supervisor port.
  • 1200: Uses 1200 baud only. This value is not recommended and may not be allowed on some devices.
  • 9600: Uses 9600 baud only. This value is the lowest standard MS/TP baud rate.
  • 19200: Uses 19200 baud only. This value is not recommended.
  • 38400: Uses 38400 baud only. This value is the recommended baud rate for bus supervisor ports.
  • 76800: Uses 76800 baud only.

Device Type

     

Disable Automatic Alarming

C,W

False

False

True

FC Bus MAC Address

     

Instance Number

     

MAC Address

C

 

1–255

Network Address

C,W

0

1–65,534

0 = Local network

65,535 = Reserved for broadcast

Offline

     

SA Bus MAC Address

   

This attribute applies to AI, AO, BI, BO, and Accumulator objects.

Slot

   

This attribute applies to AI, BI, and Accumulator objects.

Slot A

   

This attribute applies to AO and BO objects.

Slot B

   

This attribute applies to PAO and BO objects.

Trunk Number