Hardware Tab - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

The Hardware tab shows hardware-related attributes associated with the hardware source of an integration, device, or a point (for example, when an object has a reference to a physical input or output).

Note: Each Hardware attribute table is organized and divided into sections of Integration Hardware attributes, Device Hardware attributes, and Point Hardware attributes (calling out when attributes are shared between these object types). These sections are indicated by headings that span across the table.