Focus Tab - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

The Focus tab appears when you define an object in the online Site Management Portal. The Focus tab shows operation attributes available for the object type to which the object belongs. The attributes displayed on the Focus tab varies by object type. For example, the Analog Input object’s Focus tab has different attributes than the Metasys server object’s Focus tab. See the specific object section for details on its Focus tab.

Note: This tab is called the Configuration tab in the SCT or in a wizard.