Diagnostic Tab - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The Diagnostic tab only appears for objects containing diagnostic data. The attributes displayed on the Diagnostic tab vary by object type. For example, the Diagnostic tab of the BACnet Protocol Engine Object has different attributes than the Engine Device Object. See the specific object section for details on its Diagnostic tab.