Associated Graphic Tab - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

The Associated Graphic tab appears when a graphic is referenced from the object using the Graphic attribute. Refer to the User Graphics Tool section in the Metasys SMP Help (LIT-1201793) for details on working with this tab.