State, Mode, and Type Sets - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

State, Mode, and Type Sets provide the source of readable text for the user interface when the displayed value can be one of many states, modes, or types. For example, the Status attribute of every object is displayed as one of the texts listed in the Object Status (Set 505).

References to specific sets appear throughout the Object Help, usually in the Values/Options/Range column of the object’s attribute table.