Object Creation - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

Objects can be created offline in the system database on the SCT and later downloaded to the host device as part of the edited database. You can also create objects online with a browser if you have the Access Privileges to configure objects using the Security Administrator System. The user interface screens and procedures are similar in either case. Creating an object involves placing it at the desired position in the Navigation Tree and defining all the attributes that are required for it to operate. The procedure begins with the Insert Menu, and a wizard guides you through all the necessary configuration steps.

See the Creating Items with Wizards section for the steps to create objects/items.