Object Help - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The Object Help describes each object in the system, the attributes of the objects, and the characteristics and functions of each attribute. The Object Help provides detailed information to aid in creating objects, entering values for configuring attributes, understanding how to read attributes, and defining the interaction between objects in regard to the attributes.