Metasys Modes - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

Metasys software can operate in two different modes: online using the Site Management Portal UI and offline using the SCT UI. When you are connected to the network engine or Metasys Server , you can perform online mode operational activities such as monitoring and commanding. When you are connected to the SCT only, you can perform offline mode system configuration tasks such as configuring point objects and features. At SCT Release 13.0, simulation mode is not supported.