Exiting - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Save changes before exiting. Exiting closes all open windows (except the Help) associated with the session, including the Alarms Window and login screen. For more information on logging out, see the Logging Out topic.

To exit, click the Exit button in the menu bar.

Note: If you are currently editing an item in a display panel, the Metasys software cancels the exit process and notifies you that you cannot exit or log out while in Edit mode. You must exit Edit mode by saving or cancelling your changes before you can exit the application.