Parameter Sheet Viewer - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

Use the Parameter Sheet Viewer to view and edit CAF file data for selected field devices. To edit CAF file data for a field device, complete the following steps:

  1. In the All Items tree, select the field device you want to view. To edit multiple field devices, hold down shift while clicking each field device.
  2. Click View > Parameter Sheet Viewer.
  3. In the Parameter Sheet window, select Parameter Sheet.
  4. Click Edit to modify CAF file data. By default, the parameter sheet displays five standard VAV CAF parameters: SA-Area, SA-KFactor, CLG-MaxFlow, CLGOCC-MinFlow, and HTGOCC-MinFlow.
  5. To create CAF parameter columns and views, select Manage Views from the View drop-down list.
Note: For information on how to edit CAF file data for an integration, see CAF Parameters.

You can use the Parameter Sheet Viewer to view and issue commands to selected field devices. You can command CAF file data after it is downloaded using the Tools > Trunk Utilities feature. For information on how to download a CAF file, see Downloading a CAF to Devices Through Trunk Utilities.

To view commands issued to a field device, complete the following steps:

  1. In the All Items tree, select the field device that you want to view. To view multiple field devices, hold down shift while clicking each field device.
  2. Click View > Parameter Sheet Viewer.
  3. In the Parameter Sheet window, select the Application Options view and switch the parameter sheet mode to Online.

To modify commands issued to a field device, complete the following steps:

  1. In the Application Options view, select the desired devices and click Edit to open the Trunk Utilities wizard. The Commands radio button is automatically selected.
  2. Specify the Commands and the Connection Type and click Next.
    Note: Select one command to perform against selected devices. For an overview of connection parameters and command features, see Downloading a CAF to Devices Through Trunk Utilities.
  3. Verify that the correct devices are selected and click Next.
  4. Enter the connection parameters specific to your connection type and click Next.
  5. Validate the information in the Trunk Utilities Summary window and click Finish.
Note: For information about how to command CAF file data for an integration see CAF Parameters.