Display Frame Layout - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The user interface allows you to define your own display frame layout. Six options are available:

Figure 1. Panel Layout Options

To change the way the panels are arranged, see Changing the Display Panel Layout. If you have a multi-panel display and you change to a layout with fewer panels, the locked items/newest items in the view stay, depending on how many panes are available in the new layout. The other panels close, and they do not reappear if you switch back to the multi-pane view.

To resize the panels, drag the borders of the panel until it reaches the desired size. To make one panel (in a multi-panel arrangement), take up the entire Display frame temporarily, click the maximize button. To restore a maximized panel in a multi-pane view, click the restore button. A panel can also be maximized/restored by double-clicking its header bar.