Launching the ActionQ - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Note: You must be in offline mode (SCT) to access the ActionQ. The ActionQ automatically launches after the Load wizard completes.

To launch the ActionQ Interface, select ActionQ from the View menu.