ActionQ Operation - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

About this task

The ActionQ shows the status of jobs and allows you to monitor, enable, disable, delete, or reschedule jobs. At Release 12.0 the improved ActionQ infrastructure provides you with more detailed statuses and additional information in the log file entries. The updated ActionQ Log file can be found under C:\ProgramData\JohnsonControls\MetasysIII\Diagnostics\ActionQueue

See the ActionQ Interface section. The ActionQ receives a job from one of the software wizards and executes the command based on the date, time, and other resource specific parameters.

The order of operation is as follows:

Procedure

  1. The ActionQ receives a job from the Manage Archive wizard with a time to start (now or in the future).
  2. The ActionQ initiates the job (for example, starts the Upload process) at the specified start time.
  3. The ActionQ interface displays the progress and final status of the job.

    Notes: