Trunk Utilities - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The Trunk Utility functionality previously only available in the NAE Point Schedule and CCT, is now integrated within SCT. This powerful feature allows you to transfer field controller files via NAE pass-through to MSTP or IP devices, transfer files with direct Ethernet connection for IP devices, or transfer files with a MAP 4.2 connection.

Note: IP field controllers do not support a BTCVT connection type or an integration through the legacy NAE Point Schedule.

The Trunk Utilities feature supports viewing and editing device parameters on field controller trunks. Parameters can be edited in offline or online mode. Along with the ability to view and edit device parameter options, Trunk Utilities also has an enhanced download workflow which provides the ability to modify, command, and view the status of, field controllers on a live system. For additional information see the CAF Parameters section or visit uLearn at https://jcpublic.kzoplatform.com/library to watch educational videos.