Archive Database Creation - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Use SCT to create a new archive database offline. To create a new archive database, copy an existing archive database, or generate a new archive database. Then add or edit information and references to sites, controllers, communications trunks, and objects (such as schedules, energy management objects, and operators).

You can also generate a database online in a single engine and upload the information to SCT for editing and archiving. See Archive Database Creation.