Archive Database - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

An archive database holds the configuration information for the field devices and field points that make up a single site or multiple sites. The archive database contains information about controllers, input/output points, alarms, and device certificates. A single server can contain multiple SCT archive databases, Configuration Data, SCT Summary Definitions, and Controller Templates.