HVAC PRO Naming Recommendations - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Use the following list of naming conventions to assist you while naming your controllers. If you follow these recommendations, 61 additional characters are available.

  • Choose a site name under 15 characters.

  • Choose a device name (network name) under 15 characters.

  • Leave the default N2 Trunk name unchanged, so it only consists of 10 characters (for example, N2 Trunk 1 or N2 Trunk 2).

  • Choose a controller’s name under 15 characters.