Edit CAF in Archive - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Select Tools > Field Device Tools > Edit CAF in Archive to modify a CAF in CCT and update the archive with these changes.

Note: To use this feature, you must install both CCT and the SCT on the local computer. If you connect to a remote installation of the SCT, you cannot use this feature.

After the CAF opens in CCT, the status Archive-Connected appears in the status bar. If you close the CAF or choose to disconnect from the archive, you invalidate the Archive-Connected state and, when saved, the CAF is not written back to the archive. You can use CCT to save a copy of the CAF and retain the Archive-Connected state.