Controller Configuration Tool (CCT) - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

You can use CCT to configure, simulate, load, and commission devices on an MS/TP bus. The list of devices that you can configure in CCT includes CVMs, CGMs, FECs, FACs, IOMs, NCEs, NIE29s, VMA16s, and VAVs. You can operate CCT in three modes of operation that provide key functionality for your system: Configuration, Simulation, and Commissioning.