Field Device Tools - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

You can commission N2 devices remotely from SCT using the Passthru mode. To perform Passthru, N2 configuration tools must reside on the computer with an SCT installed. You can launch Passthru applications from SCT or the online Metasys Site Management Portal UI. In addition, you can attach resource files, which are files created by N2 configuration tools, to field devices as extensions to assist with generating and mapping field points. See Table 1 for the file extension of the legacy tools supported by the engine.

Note: The File Name Expected during Import is the file required by the N2 Integration import utility for generating XML. The original Configuration Tool files are not stored in the engine.
Table 1. Supported Legacy Tools

Device/Controller Type

Configuration Tool (M-Tool)

File Name Expected during Import

ASC

HVAC PRO, LoaderUI

PRN

Note: When generating PRN files from the HVAC PRO, use the long format.

VMA

HVAC PRO

PRN

Vendor

Vendor

PRN

XP

XTM Configurator, LoaderUI

HMC

DX

GX-9100 Tool, LoaderUI DX Commissioning Tool

DMO

MIG

Metasys Integrator unit

VCT